Booting ADS5121 board (mpc5121e) with NFS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Booting ADS5121 board (mpc5121e) with NFS

ソリューションへジャンプ
3,715件の閲覧回数
bbjh1
Contributor I

Hi,

 

I am trying to boot the ads5121 board using NFS. I restarted the NFS server and teh output is shown in the attached txt file nfs server.txt.

I also printed the env in u-boot and the output is found in the attached file u-boot.txt.

When I tried to boot the board with the nfs option I ot an error. The output is shown in the attached file nfsrun.txt.

 

My host machine is running under Centos 4.7 and my target is the ads512101 board rev 3.0.  I installed the BSP from the LTIB iso file found on freescale.com (MPC512xADS_20090603-ltib.iso). I am guessing that maybe the ltib file is the worng one.

Can someone please help me?

Thank you in advance.

0 件の賞賛
返信
1 解決策
2,284件の閲覧回数
moidom
Contributor II

Hi¡

 

Have you followed steps of MPC5121 Porting Linux app note ?

 

http://www.freescale.com/files/32bit/doc/app_note/AN3765.pdf

 

Is very good explained, tell me about problems.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,285件の閲覧回数
moidom
Contributor II

Hi¡

 

Have you followed steps of MPC5121 Porting Linux app note ?

 

http://www.freescale.com/files/32bit/doc/app_note/AN3765.pdf

 

Is very good explained, tell me about problems.

0 件の賞賛
返信
2,284件の閲覧回数
bbjh1
Contributor I

Moidom,

 

I followed the steps in AN3765.pdf up till Section 2.3. Do I have to follow the other sections?

I already replied to your reply on my other thread

 

https://community.freescale.com/thread/64183

 

If you have time please I would really appreciate your help. Thank you.

 

bbjh1

0 件の賞賛
返信
2,284件の閲覧回数
moidom
Contributor II

From pages 34 to 42

0 件の賞賛
返信