The input image formats supported by the Parallel CSI block on the i.MX RT1050 processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The input image formats supported by the Parallel CSI block on the i.MX RT1050 processor

Jump to solution
856 Views
dhy
Contributor I

Hello.

We are considering using the I.MX RT1050.

Could you please confirm if the Parallel-CSI supports YC16 (16-bit) interface and YUV4:2:2 packed format (YUYV) as inputs?


Thank you in advance for your assistance.

 

0 Kudos
Reply
1 Solution
842 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @dhy,

The supported inputs for the CSI module are listed on "Table 34-2. CSI input data format" from the RT1050 Reference Manual. Please look into this table and let me know if you have any further inquiries.

BR,
Edwin.

View solution in original post

0 Kudos
Reply
1 Reply
843 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @dhy,

The supported inputs for the CSI module are listed on "Table 34-2. CSI input data format" from the RT1050 Reference Manual. Please look into this table and let me know if you have any further inquiries.

BR,
Edwin.

0 Kudos
Reply