The input image formats supported by the Parallel CSI block on the i.MX RT1050 processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

The input image formats supported by the Parallel CSI block on the i.MX RT1050 processor

跳至解决方案
848 次查看
dhy
Contributor I

Hello.

We are considering using the I.MX RT1050.

Could you please confirm if the Parallel-CSI supports YC16 (16-bit) interface and YUV4:2:2 packed format (YUYV) as inputs?


Thank you in advance for your assistance.

 

0 项奖励
回复
1 解答
834 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @dhy,

The supported inputs for the CSI module are listed on "Table 34-2. CSI input data format" from the RT1050 Reference Manual. Please look into this table and let me know if you have any further inquiries.

BR,
Edwin.

在原帖中查看解决方案

0 项奖励
回复
1 回复
835 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @dhy,

The supported inputs for the CSI module are listed on "Table 34-2. CSI input data format" from the RT1050 Reference Manual. Please look into this table and let me know if you have any further inquiries.

BR,
Edwin.

0 项奖励
回复