The abnormal output in the test of SJA1124AHG terminate resistor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The abnormal output in the test of SJA1124AHG terminate resistor

ソリューションへジャンプ
1,288件の閲覧回数
xuelong
Contributor I

Hi NXP expert,

We did a test to verify the pull up resistor of SJA1124AHG. The test steps are as follows:

1. The test setup is showed in the attached picture, Rtest = 1Kohm;

2. Turn off SW1(disconnect Rtest), get the recessive signal voltage V1;

3, Turn on SW1(connect Rtest), get the recessive signal voltage V2;

4, The pull up resistor of SJA1124AHG will be calculated: Rterminate = Rtest (V1/V2–1).

12343.PNGHowever, in the test, when disconnected Rtest, SJA1124AHG has a normal output:

LIN3_V1.pngBut when the Rtest is connected, no any output signal will be detected:

LIN3_V2.pngDoes SJA1124AHG could not support 1K load? please help us to analysis this.

And this test method is implement on TJA1021, TJA1021 works well.

タグ(1)
0 件の賞賛
返信
1 解決策
1,262件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Chen,

The integrated LIN commander pull-up resistor in the SJA1124A is 1Kohm. However, the integrated LIN commander pull-up is protected against too long dominant times. See below snapshot from the data sheet.

image006 (3).png

image007 (1).png

For the LIN commander pull-up resistor value measurement, an external pull-down resistor should be chosen that keeps the LIN signal recessive. For instance, Rtest=2kohm will result in 66% Vbat, which is still LIN recessive.

BR, Tomas

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,263件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Chen,

The integrated LIN commander pull-up resistor in the SJA1124A is 1Kohm. However, the integrated LIN commander pull-up is protected against too long dominant times. See below snapshot from the data sheet.

image006 (3).png

image007 (1).png

For the LIN commander pull-up resistor value measurement, an external pull-down resistor should be chosen that keeps the LIN signal recessive. For instance, Rtest=2kohm will result in 66% Vbat, which is still LIN recessive.

BR, Tomas

 

0 件の賞賛
返信
1,241件の閲覧回数
xuelong
Contributor I

Got it, thank you so much, Tomas!

0 件の賞賛
返信