TJA1145 - Wakeup not happening as expected

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1145 - Wakeup not happening as expected

Jump to solution
3,781 Views
maitreya_jain
Contributor I

We are using TJA1145 High-speed CAN transceiver for partial networking. The selective wakeup is configured. But it is observed that the transceiver wakeup do not happen with first frame. But on receiving the second frame the wakeup is successful.  Also if there is a significant delay between the first and second frame (two frames must be received within 1sec) also the transceiver do not wakeup. Could you please help us in this regard.

Tags (2)
1 Solution
3,010 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this could be caused by Autonomous CAN biasing. The device only terminates its CAN bus pins to GND while

- the CAN block is in a low-power mode and

- the bus is idle for longer than approximately one second.

Otherwise the CAN bus pins bias towards 2,5V.

Each time there is traffic on the bus (see Fig 9) an internal timer is reset and the bus pins bias towards 2,5V. At bus silence the timer starts counting until about one second. After this silence time the bus biasing changes towards 0V.

 pastedImage_1.png

So the first frame is not probably received without error due to GND biasing and also makes bus biasing to 2.5V again.

Then if second frame is received within about one second, the transceiver wakeup normally.

 

See TR1309 Application Hints - High speed CAN transceiver for partial networking TJA1145 (http://www.nxp.com/documents/report/AH1309_v1_1_Application_Hints_TJA1145.pdf) for mor info about this transceiver.

BR, Petr

View solution in original post

2 Replies
3,011 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this could be caused by Autonomous CAN biasing. The device only terminates its CAN bus pins to GND while

- the CAN block is in a low-power mode and

- the bus is idle for longer than approximately one second.

Otherwise the CAN bus pins bias towards 2,5V.

Each time there is traffic on the bus (see Fig 9) an internal timer is reset and the bus pins bias towards 2,5V. At bus silence the timer starts counting until about one second. After this silence time the bus biasing changes towards 0V.

 pastedImage_1.png

So the first frame is not probably received without error due to GND biasing and also makes bus biasing to 2.5V again.

Then if second frame is received within about one second, the transceiver wakeup normally.

 

See TR1309 Application Hints - High speed CAN transceiver for partial networking TJA1145 (http://www.nxp.com/documents/report/AH1309_v1_1_Application_Hints_TJA1145.pdf) for mor info about this transceiver.

BR, Petr

2,159 Views
chenhuang
Contributor II
 
0 Kudos
Reply