[TJA1027] question about RXD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[TJA1027] question about RXD

3,485件の閲覧回数
bradlin1
Contributor I

I would like to connect TJA1027 LIN controller to a 3.3V interface on a FPGA. The datasheet shows the following application diagram. To work with a 3.3V FPGA interface, do I just need to add a pull the RXD signal (open-drain output) to 3.3V, not matter of the VBAT voltage on the other side of TJA1027? If this is correct, what pull-up resistance value should I use?

Is there anything else I need to to on TXD and SLP_N signals (input)?

Thanks!#

NXP_TJA-1027_LIN_diagram.jpg

タグ(1)
0 件の賞賛
返信
1 返信

3,383件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Please read about attached file page18-20 for your questions.

0 件の賞賛
返信