[TJA1027] question about RXD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[TJA1027] question about RXD

3,486 Views
bradlin1
Contributor I

I would like to connect TJA1027 LIN controller to a 3.3V interface on a FPGA. The datasheet shows the following application diagram. To work with a 3.3V FPGA interface, do I just need to add a pull the RXD signal (open-drain output) to 3.3V, not matter of the VBAT voltage on the other side of TJA1027? If this is correct, what pull-up resistance value should I use?

Is there anything else I need to to on TXD and SLP_N signals (input)?

Thanks!#

NXP_TJA-1027_LIN_diagram.jpg

Tags (1)
0 Kudos
Reply
1 Reply

3,384 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Please read about attached file page18-20 for your questions.

0 Kudos
Reply