TFTP timeout error for custom Board based on LS1046ardb using LSDK 21.08

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TFTP timeout error for custom Board based on LS1046ardb using LSDK 21.08

Jump to solution
3,642 Views
Ghouse
Contributor V

Hi,

Iam using a custom board based on LS1046ardb, attached is the boot log.

When iam trying to copy the qspi image file using tftp, the tftp is getting timed out and iam not able to copy the img.

Please note that with the same tftp server settings and image built on LSDK 20.04 iam able to successfully copy using the image, but when i build image using LSDK 21.08 iam facing this tftp issue.

Please let me know what to do.

Thank u.

0 Kudos
Reply
1 Solution
3,625 Views
Ghouse
Contributor V

Hi,

yes , i have added "CONFIG_PHY_MARVELL=y" in configs/ls1046ardb_tfa_defconfig in u-boot source code

View solution in original post

0 Kudos
Reply
4 Replies
3,628 Views
yipingwang
NXP TechSupport
NXP TechSupport

Have you added "CONFIG_PHY_MARVELL=y" in configs/ls1046ardb_tfa_defconfig in u-boot source code?

0 Kudos
Reply
3,626 Views
Ghouse
Contributor V

Hi,

yes , i have added "CONFIG_PHY_MARVELL=y" in configs/ls1046ardb_tfa_defconfig in u-boot source code

0 Kudos
Reply
3,594 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please diff configs/ls1046ardb_tfa_defconfig between LSDK 20.04 and LSDK 21.08 to find the different setting.

0 Kudos
Reply
3,565 Views
Ghouse
Contributor V

Hi, i compared ls1046ardb_tfa_defconfig between LSDK 20.04 and LSDK 21.08 and reverted few of the parameters to old, and it started working.

Thank u.

 

0 Kudos
Reply