TFTP timeout error for custom Board based on LS1046ardb using LSDK 21.08

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TFTP timeout error for custom Board based on LS1046ardb using LSDK 21.08

跳至解决方案
3,640 次查看
Ghouse
Contributor V

Hi,

Iam using a custom board based on LS1046ardb, attached is the boot log.

When iam trying to copy the qspi image file using tftp, the tftp is getting timed out and iam not able to copy the img.

Please note that with the same tftp server settings and image built on LSDK 20.04 iam able to successfully copy using the image, but when i build image using LSDK 21.08 iam facing this tftp issue.

Please let me know what to do.

Thank u.

0 项奖励
回复
1 解答
3,623 次查看
Ghouse
Contributor V

Hi,

yes , i have added "CONFIG_PHY_MARVELL=y" in configs/ls1046ardb_tfa_defconfig in u-boot source code

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,626 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Have you added "CONFIG_PHY_MARVELL=y" in configs/ls1046ardb_tfa_defconfig in u-boot source code?

0 项奖励
回复
3,624 次查看
Ghouse
Contributor V

Hi,

yes , i have added "CONFIG_PHY_MARVELL=y" in configs/ls1046ardb_tfa_defconfig in u-boot source code

0 项奖励
回复
3,592 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please diff configs/ls1046ardb_tfa_defconfig between LSDK 20.04 and LSDK 21.08 to find the different setting.

0 项奖励
回复
3,563 次查看
Ghouse
Contributor V

Hi, i compared ls1046ardb_tfa_defconfig between LSDK 20.04 and LSDK 21.08 and reverted few of the parameters to old, and it started working.

Thank u.

 

0 项奖励
回复