TEF8101 ADC data error?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TEF8101 ADC data error?

Jump to solution
2,292 Views
longfeiwang
Contributor III

I am using TEF8101 (LVDS interface),When I set the decimation rate to 1, the ADC equivalent sampling rate is 40MHZ,The ADC data (DC component 2048 has been subtracted) seems to have a lot of sudden changes(-2048\-2045...), such as the figure below.

longfeiwang_0-1617008931472.png

 

If I change the decimation rate to 2 and the equivalent sampling rate is 20MHZ, the abrupt data will not exist.

Has some filtering been done in the PDC?

 

0 Kudos
Reply
1 Solution
2,276 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Could you please explain what your are intending to do?

Decimation factor of 1 is for test purposes only, as stated in the datasheet

petervlna_0-1617090222534.png

 

Best regards,

Peter

View solution in original post

0 Kudos
Reply
2 Replies
2,277 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Could you please explain what your are intending to do?

Decimation factor of 1 is for test purposes only, as stated in the datasheet

petervlna_0-1617090222534.png

 

Best regards,

Peter

0 Kudos
Reply
2,273 Views
longfeiwang
Contributor III

The problem has been solved. After modifying the FPGA LVDS timing, the abrupt data no longer exists

0 Kudos
Reply