TEA1916 inrush current startup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TEA1916 inrush current startup

ソリューションへジャンプ
2,644件の閲覧回数
juliocruz
Contributor III

Hello,

A power supply based on the evaluation board (TEA1916DB1262 is getting high inrush current when the cable is connected, creating sparks and issues in the system.

I tried adjusting Rgate as suggested in TRM (10.1 Setting the soft start power level) but the results are similar. In fact, after changing from 180K to 120K, two (2) boards units get damaged (SUPIC is ~4.22V).

Below some questions:

  • What could get wrong after changing Rgate from 180K to 120K that the boards get damaged? 
  • Which others settings are affected when Rgate is changed?
  • During the startup, how to limit the current on the the boost capacitor (C115) of the evaluation board? 
  • What is the function of the diode D105 in the evaluation board? This could be causing the inrush reported on this test?

Appreciated any suggestion in this regards,

Thanks

タグ(2)
1 解決策
2,558件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

 Various Rgate will bring effect on expected start frequency,if use 120K there is 300Khz,if 180K will bring 180Khz.

In the start up the D105 is shunt diode. D105 will protect the PFC MOSFET ( forbid large current flow into L104 then saturation)

元の投稿で解決策を見る

2 返答(返信)
2,558件の閲覧回数
juliocruz
Contributor III

Dear guoweisun‌, please, may you take a look to the questions in this post related with the inrush current? Thanks

0 件の賞賛
返信
2,559件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

 Various Rgate will bring effect on expected start frequency,if use 120K there is 300Khz,if 180K will bring 180Khz.

In the start up the D105 is shunt diode. D105 will protect the PFC MOSFET ( forbid large current flow into L104 then saturation)