Simulation in Keysight ADS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Simulation in Keysight ADS

ソリューションへジャンプ
2,050件の閲覧回数
pumpkin
Contributor I

Hello,

I want to simulate an amplifier by using the NXP MRFE6VP5150. Therefore I used the ADS Model from NXP. I have obtained fixed line lengths through my simulation.
As far as I know, a length is defined from the center of a pad to the center of the next pad. This would mean that my signal path on the pcb is shorter at the end than what is given in the simulation, because the signal path would stop before the transistor pad. This would also mean, that the NXP Model only includes half of the pad from the transistor.
The other possibility would be, that the length stops before the pad of the transistor begins, which would mean that the ADS Model from NXP includes the pad till the end.

So how is it correct?

Thank you very much in advance!

0 件の賞賛
返信
1 解決策
2,035件の閲覧回数
ErikaC
NXP TechSupport
NXP TechSupport

Hello, NXP Model only includes half of the pad from the transistor.

Regards

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,012件の閲覧回数
pumpkin
Contributor I

Thanks a lot!

0 件の賞賛
返信
2,036件の閲覧回数
ErikaC
NXP TechSupport
NXP TechSupport

Hello, NXP Model only includes half of the pad from the transistor.

Regards

 

0 件の賞賛
返信