SJA1105TEL MAC Configuration Table (block 09h)、PHY Address

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SJA1105TEL MAC Configuration Table (block 09h)、PHY Address

ソリューションへジャンプ
1,405件の閲覧回数
haiyang
Contributor III

hi,

i use SJA1105TEL to design a Ethenter Switch;

1、if i set the MAC Configuration Table (block 09h)  all the TOP 、BASE、ENABLE field to  0;

what will happen?

2、if set port0 port1 in phy mode ,how to set the phy address? 

thanks

haiyang

タグ(1)
0 件の賞賛
返信
1 解決策
1,352件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

PHY address is for SMI bus. This can be set on PHY like TJA110x, for example and it is used for host CPU to communicate with the PHY. SJA1105 working in PHY mode (MAC-MAC) doesn't have SMI and doesn't need such address.

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,387件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @haiyang 
In case any queue is not enabled for a port, the forwarded frame which is assigned to this queue is dropped.
Regards,
Lukas

0 件の賞賛
返信
1,382件の閲覧回数
haiyang
Contributor III

hi,

thanks reply ,i see your point!

and the second question ,how to set 

the phy address for port0 and port1, when they set to phy mode?

in my memory,the SJA1105P  can set address through some config pin,but the 

SJA1105TEL have no these pin

best wish

haiyang

0 件の賞賛
返信
1,353件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

PHY address is for SMI bus. This can be set on PHY like TJA110x, for example and it is used for host CPU to communicate with the PHY. SJA1105 working in PHY mode (MAC-MAC) doesn't have SMI and doesn't need such address.

Regards,

Lukas

0 件の賞賛
返信