SJA1105TEL MAC Configuration Table (block 09h)、PHY Address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SJA1105TEL MAC Configuration Table (block 09h)、PHY Address

Jump to solution
1,403 Views
haiyang
Contributor III

hi,

i use SJA1105TEL to design a Ethenter Switch;

1、if i set the MAC Configuration Table (block 09h)  all the TOP 、BASE、ENABLE field to  0;

what will happen?

2、if set port0 port1 in phy mode ,how to set the phy address? 

thanks

haiyang

Tags (1)
0 Kudos
Reply
1 Solution
1,350 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

PHY address is for SMI bus. This can be set on PHY like TJA110x, for example and it is used for host CPU to communicate with the PHY. SJA1105 working in PHY mode (MAC-MAC) doesn't have SMI and doesn't need such address.

Regards,

Lukas

View solution in original post

0 Kudos
Reply
3 Replies
1,385 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @haiyang 
In case any queue is not enabled for a port, the forwarded frame which is assigned to this queue is dropped.
Regards,
Lukas

0 Kudos
Reply
1,380 Views
haiyang
Contributor III

hi,

thanks reply ,i see your point!

and the second question ,how to set 

the phy address for port0 and port1, when they set to phy mode?

in my memory,the SJA1105P  can set address through some config pin,but the 

SJA1105TEL have no these pin

best wish

haiyang

0 Kudos
Reply
1,351 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

PHY address is for SMI bus. This can be set on PHY like TJA110x, for example and it is used for host CPU to communicate with the PHY. SJA1105 working in PHY mode (MAC-MAC) doesn't have SMI and doesn't need such address.

Regards,

Lukas

0 Kudos
Reply