SDMMC example for RW612 module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDMMC example for RW612 module

ソリューションへジャンプ
1,785件の閲覧回数
khalidL
Contributor II

The current RW612 SDK version doesn't include a startup example related to interfacing an SD card (SDMMC Example). Is there any tutorial or example that can be imported from other project to implement an SD file system using the RW612 module?

We appreciate your help and time.

0 件の賞賛
返信
1 解決策
1,760件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

 

I'm sorry for the inconvenience.

I looked at the datasheet of the EVK-IRIS-W1 and in page 15, it states the following SDIO information "SDIO as peripheral only".

The SDIO can be used for the NCP application using another MCU or MPU as host. For instance, an i.MX RT1060 manages the application code while RW612 handles Wi-Fi, Bluetooth Low Energy, and IEEE 802.15.4 stacks. You can find more information regarding this in UM12133 and UM12095.

 

Regards,

Daniel.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,772件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

 

The RW612 SDIO interface can only work in slave mode.

 

Regards,

Daniel.

0 件の賞賛
返信
1,765件の閲覧回数
khalidL
Contributor II

Hi Daniel,

Thank you for your quick reply, I though so, since there was no related info for host configuration in the Datasheet, but the UBLOX dev board (IRIS-W101) using the RW612 are connecting an SD Card to this bus!!!!.

0 件の賞賛
返信
1,761件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

 

I'm sorry for the inconvenience.

I looked at the datasheet of the EVK-IRIS-W1 and in page 15, it states the following SDIO information "SDIO as peripheral only".

The SDIO can be used for the NCP application using another MCU or MPU as host. For instance, an i.MX RT1060 manages the application code while RW612 handles Wi-Fi, Bluetooth Low Energy, and IEEE 802.15.4 stacks. You can find more information regarding this in UM12133 and UM12095.

 

Regards,

Daniel.

0 件の賞賛
返信
1,710件の閲覧回数
khalidL
Contributor II
Got it.
Thanks.
0 件の賞賛
返信