SDMMC example for RW612 module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDMMC example for RW612 module

Jump to solution
1,784 Views
khalidL
Contributor II

The current RW612 SDK version doesn't include a startup example related to interfacing an SD card (SDMMC Example). Is there any tutorial or example that can be imported from other project to implement an SD file system using the RW612 module?

We appreciate your help and time.

0 Kudos
Reply
1 Solution
1,759 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

 

I'm sorry for the inconvenience.

I looked at the datasheet of the EVK-IRIS-W1 and in page 15, it states the following SDIO information "SDIO as peripheral only".

The SDIO can be used for the NCP application using another MCU or MPU as host. For instance, an i.MX RT1060 manages the application code while RW612 handles Wi-Fi, Bluetooth Low Energy, and IEEE 802.15.4 stacks. You can find more information regarding this in UM12133 and UM12095.

 

Regards,

Daniel.

View solution in original post

0 Kudos
Reply
4 Replies
1,771 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

 

The RW612 SDIO interface can only work in slave mode.

 

Regards,

Daniel.

0 Kudos
Reply
1,764 Views
khalidL
Contributor II

Hi Daniel,

Thank you for your quick reply, I though so, since there was no related info for host configuration in the Datasheet, but the UBLOX dev board (IRIS-W101) using the RW612 are connecting an SD Card to this bus!!!!.

0 Kudos
Reply
1,760 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

 

I'm sorry for the inconvenience.

I looked at the datasheet of the EVK-IRIS-W1 and in page 15, it states the following SDIO information "SDIO as peripheral only".

The SDIO can be used for the NCP application using another MCU or MPU as host. For instance, an i.MX RT1060 manages the application code while RW612 handles Wi-Fi, Bluetooth Low Energy, and IEEE 802.15.4 stacks. You can find more information regarding this in UM12133 and UM12095.

 

Regards,

Daniel.

0 Kudos
Reply
1,709 Views
khalidL
Contributor II
Got it.
Thanks.
0 Kudos
Reply