SC18IM704 UART message rate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SC18IM704 UART message rate

1,408件の閲覧回数
Tix00
Contributor II

Hi to everyone! wich is the maximum message rate (I2C transactions) for this IC?

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,383件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Vicent,

The I2C clock rate is configurable via I2CClkL and I2CClkH registers and can be set up to 375 kHz.

Capture.JPG

BR, Tomas

0 件の賞賛
返信

1,380件の閲覧回数
Tix00
Contributor II

Hi Tomas, thanks for your fast reply.

Your table referes to I2C bus clock frequency, but my question is about the overall IC capacity for processing UART messages to the I2C machine. I mean to send a simple (two bytes) SxxxxxxP I2C write [not waiting for an answer] command message to the UART interface and dump it to the I2C bus.

Thank you in advance!

0 件の賞賛
返信