SC16IS750 software reset does not work in SPI mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SC16IS750 software reset does not work in SPI mode?

Jump to solution
2,875 Views
shinoda
Contributor I

I have a software that drives an SC16IS750 in both I2C and SPI modes. The SC16IS750 works great in both modes except for one single problem. That is, "SC16IS750 does not seem to respond to software reset bit (SRESET) written to  IOControl[3] in SPI mode".

After writing 1 to this bit, all registers remain unchanged.

It does respond to the very same process in I2C mode, and registers are initialized as described in the "7.4.1 Hardware reset, Power-On Reset (POR) and software reset".

Have any information on this phenomenon?

0 Kudos
Reply
1 Solution
2,315 Views
shinoda
Contributor I

Tomas,

Thanks for the comment.

Actually, the problem was self solved.

It was caused by the wrong bus mode. The chip should have been operated with CPOL=0 and CPHA=0 (aka mode 0), but my driver was using CPOL=1 and CPHA=1 (aka mode 3).

It's super amazing that rest of the driver works perfectly with mode 3, sending and writing continuously using fifo; the IOControl register was the only register I couldn't write/read correctly.

View solution in original post

0 Kudos
Reply
2 Replies
2,316 Views
shinoda
Contributor I

Tomas,

Thanks for the comment.

Actually, the problem was self solved.

It was caused by the wrong bus mode. The chip should have been operated with CPOL=0 and CPHA=0 (aka mode 0), but my driver was using CPOL=1 and CPHA=1 (aka mode 3).

It's super amazing that rest of the driver works perfectly with mode 3, sending and writing continuously using fifo; the IOControl register was the only register I couldn't write/read correctly.

0 Kudos
Reply
2,315 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Yoichi,

I have not heard of such a problem before and I am asking our product group to comment on this.

Meanwhile, could you please post here a screenshot illustrating the SPI transfer when writing to the IOControl register?

Regards,

Tomas

0 Kudos
Reply