S32S Code Profiling timings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32S Code Profiling timings

3,859件の閲覧回数
NAA524534
Contributor II

Hi,

We wanted to check if you have any code profile timings values for base drivers available? This is to do timing analysis. If Approximate estimations available also, kindly share .

 

0 件の賞賛
返信
5 返答(返信)

3,795件の閲覧回数
NAA524534
Contributor II

Hi,

Thank you for the explanation. We don't have the micro controller with us yet. Is it possible to analyze without a target?

0 件の賞賛
返信

3,783件の閲覧回数
Lambert_Yang
NXP Employee
NXP Employee

Hi,

It's possible to use an emulator to do that but I don't know if it's available for customers. Please reach out to the NXP contact (sales/FAE/disty) of your company for details.

0 件の賞賛
返信

3,763件の閲覧回数
NAA524534
Contributor II

Hi,

Is it possible to share information information/manual on emulator?

0 件の賞賛
返信

3,761件の閲覧回数
Lambert_Yang
NXP Employee
NXP Employee

Sorry, I don't have it. Please kindly ask for help from your company's NXP contact person. Thank you.

0 件の賞賛
返信

3,812件の閲覧回数
Lambert_Yang
NXP Employee
NXP Employee

Hi Neetigya,

We don't have specific code for measuring S32S247 driver timing. But it's not hard to do that for users.

When doing timing analysis, it's common to use a timer, like STM, to measure time. Compare the timer counter between the starting point and ending point.

This is the basic method for analyzing code efficiency, interrupt firing, core loading, etc.

There are timer examples in the S32S247 SDK package, you can port the code to where you want to do timing analysis.

タグ(2)
0 件の賞賛
返信