[S32R294] Cannot view the EmbSys Register View for S32R294.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[S32R294] Cannot view the EmbSys Register View for S32R294.

ソリューションへジャンプ
2,483件の閲覧回数
Gordon_Yang
Contributor III

My S32DS cannot look up the register table.

And in the "EmbSys Register View" window, it shows that "SVD descriptor not found for project PF294_Z4_0".

But I have set the register view to chip S32R294. How should I resolve this problem? Thanks.

Gordon_Yang_0-1620804182419.png

Gordon_Yang_1-1620804200115.png

 

 

0 件の賞賛
返信
1 解決策
2,474件の閲覧回数
Gordon_Yang
Contributor III

I removed the project files ".metadata". And recreated another project file with the same source codes. It worked.

I'm not sure whether it is IDE's bug or not.

Gordon_Yang_0-1620809455563.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,467件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Nice to hear that.

Always try fresh project to verify if it is not any configuration/modification issue.

Best regards,

Peter

2,475件の閲覧回数
Gordon_Yang
Contributor III

I removed the project files ".metadata". And recreated another project file with the same source codes. It worked.

I'm not sure whether it is IDE's bug or not.

Gordon_Yang_0-1620809455563.png

 

0 件の賞賛
返信