Request for Support – Output Shorting Issue After Pulling Up Power-On Pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Request for Support – Output Shorting Issue After Pulling Up Power-On Pin

1,702 Views
Shivani_Elavena
Contributor III

 

Hello Jozef,

I am facing an issue with one of our designs and would appreciate your guidance.

We have pulled up the POWER_ON pin as per the requirement, but after doing this, we are observing that the output pins appear to be shorted (or are behaving as if they are shorted). We are not able to understand the root cause of this behaviour.

Could you please help us understand:

  1. Why the outputs become shorted after pulling up the POWER_ON pin?

  2. Whether there are any specific configuration steps or hardware conditions required for this pin?

  3. Any recommended diagnostics or checks to isolate the issue?

If needed, I can provide the schematic snippet or measurement screenshots.

Thank you in advance for your support.

Regards,
Shivani e.

0 Kudos
Reply
3 Replies

1,574 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Shivani,

please share your schematic with voltage levels and part values. Is the issue repeatable? On how many boards do you see this issue? If you replace the PF5020 for a new piece, is the behavior the same? 

With Best Regards,

Jozef

 

0 Kudos
Reply

1,659 Views
Shivani_Elavena
Contributor III

Hello Veronika,

Thank you for your support.

The NXP part number we are using in our application is PF5020.

Kindly redirect this inquiry to the appropriate product team.

Thank you in advance.

Best regards,
Shivani e.

0 Kudos
Reply

1,675 Views
Veronika_techsupport
NXP TechSupport
NXP TechSupport

Hello @Shivani_Elavena 

could you please share NXP part number you are using for your application to be able to properly redirected to product team.

Thank you in advance.

Best regards