RFIDDiscover - Cannot Update the PCSC Reader List

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RFIDDiscover - Cannot Update the PCSC Reader List

ソリューションへジャンプ
5,518件の閲覧回数
vince1
Contributor III

I am using RFIDDiscoverV4.10.0.0 on a Windows 10 PC.

I am trying to update the "PCSC Reader List" to use a SpringCard PC/SC readers as explained here.

https://tech.springcard.com/2021/using-nxp-rfiddiscover-with-springcard-pc-sc-couplers/

I connect the SpringCard Reader to a USB port on my PC and hear the connection tone.

Then I click the Update button in the PCSC Readers (PR533,PN533 & SCM) screen, and nothing happens.  The connected PCSC Reader is not listed.  I tried this with several others PC readers with the same result (the Readers are not listed).

Do you have any suggestions?

Thanks,

Vince

ラベル(2)
0 件の賞賛
返信
1 解決策
5,512件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @vince1 ,

 

Have you tried with the following 3 readers?

  • SpringCard Puck Contactless 0
  • SpringCard Prox'N'Roll Contactless 0
  • SpringCard SpringPark Contactless 0

They are mentioned from https://tech.springcard.com/2021/using-nxp-rfiddiscover-with-springcard-pc-sc-couplers/ and should be able to work with RFIDDiscoverV4.10.0.0 . 

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
5,513件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @vince1 ,

 

Have you tried with the following 3 readers?

  • SpringCard Puck Contactless 0
  • SpringCard Prox'N'Roll Contactless 0
  • SpringCard SpringPark Contactless 0

They are mentioned from https://tech.springcard.com/2021/using-nxp-rfiddiscover-with-springcard-pc-sc-couplers/ and should be able to work with RFIDDiscoverV4.10.0.0 . 

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

5,507件の閲覧回数
vince1
Contributor III

Thanks, I got it working.  My error was you must manually populate the fields to update the Reader List.  Now all works as expected.

0 件の賞賛
返信
5,493件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @vince1 ,

 

Great to know that! Thanks for the update!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信