RFID Discover tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
241件の閲覧回数
rreddy2
Contributor I

When I am installing the RFID discover tool, I get error(image.png) stating that setupengine.dll is not found, to resolve this I have tried few things mentioned in the online forums such as running system file checker, installing a .net framework and extension. still no luck
in the popup it is mentioned that reinstalling will resolve. but I end up with error (error2.png) when I run the application.
Please let me know how to resolve this issue.
 OS: Windows11

0 件の賞賛
返信
1 解決策
113件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

just as FYI, this has been fixed by re-installing the latest version at the moment the latest is 5.7. available inside secure files, under NDA. 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
114件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

just as FYI, this has been fixed by re-installing the latest version at the moment the latest is 5.7. available inside secure files, under NDA. 

0 件の賞賛
返信
216件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi @rreddy2 

Hope you are doing great, 

can you confirm pls which package is being used here, I want to know if you are trying to install the free one on the webpage or the full version which is the on inside secure files. 

in either cases I will get in touch with you directly, then when this is fixed I will add the answer to this post, so there is a reference for other people with the same issue. 

 

BR

 

Jonathan

0 件の賞賛
返信