Question aboout interface called in MFGTools

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Question aboout interface called in MFGTools

907 次查看
aoboyan
Contributor I

Hi,

 I have a question how i can call interface such as 'start' and 'stop' button in MSGTools. There are reason why i want to use these to control action of flash by the third part software to complete an action continuely.

Thanks

标记 (1)
0 项奖励
回复
1 回复

867 次查看
igorpadykov
NXP Employee
NXP Employee

Hi 奥博 闫 

one can use mfg tool sources for writing own application with necessary functions

GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复