Programming the OTP options on AR6000

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming the OTP options on AR6000

1,632 Views
nick_norman
Contributor I

Although the datasheet shows what options can be OTP into an AR6000 alternator regulator, I can’t see where it says how this programming is actually done by the user. Is there another document that covers the OTP programming of AR6000?

Tags (1)
0 Kudos
Reply
2 Replies

1,416 Views
devonna_dorton
NXP Employee
NXP Employee

I am looking for the programming specifications for NXP AR6000 to provide to one of our device programming partners.

0 Kudos
Reply

1,580 Views
nxf54943
NXP Employee
NXP Employee

Hello Nick,
Sorry, but the information you are requesting is treated as confidential info at this time and requires a disclaimer between your company and NXP.
Naturally, we cannot discuss this with you in public, this requires to be handled as a support ticket. In the following link you'll be able to see the steps you need to follow in order to submit one: https://community.nxp.com/docs/DOC-329745 
We will stop following this thread and contact you by email to further communicate about the technical question.

Kind regards,
Andrea

-------------------------------------------------------------------------------
Note:
This thread is continued as a private discussion with the submitter,
NXP support is not following the thread anymore
-------------------------------------------------------------------------------

0 Kudos
Reply