Programmer for WCT1013.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programmer for WCT1013.

Jump to solution
5,350 Views
stproj18
Contributor I

I need to know what programmer I can use for WCT1013. Somebody can help me?

Tags (1)
0 Kudos
Reply
1 Solution
5,048 Views
fortunely
Contributor III

Hello Flavio Caruso,

I guess you maybe need a programmer for production. 

Maybe you can use PEMicro U-Cyclone (Fx), pls refer: 

PEmicro | Experts in Embedded tools for Flash Programming and Development 

You can query all device supported from the following link:

PEmicro | Experts in Embedded tools for Flash Programming and Development  

pastedImage_3.png

It doesn't include MWCT1013, but the PC software for U-Cyclone can support it. Pls update your PC software if there is no PN MWCT1013 in your PC software.

pastedImage_4.png

View solution in original post

0 Kudos
Reply
7 Replies
5,049 Views
fortunely
Contributor III

Hello Flavio Caruso,

I guess you maybe need a programmer for production. 

Maybe you can use PEMicro U-Cyclone (Fx), pls refer: 

PEmicro | Experts in Embedded tools for Flash Programming and Development 

You can query all device supported from the following link:

PEmicro | Experts in Embedded tools for Flash Programming and Development  

pastedImage_3.png

It doesn't include MWCT1013, but the PC software for U-Cyclone can support it. Pls update your PC software if there is no PN MWCT1013 in your PC software.

pastedImage_4.png

0 Kudos
Reply
5,048 Views
stproj18
Contributor I

Hi Martin,

   Many thanks for the answer! This is exactly what I need! 

   Exist an other options too? I mean other devices like this?

Regrads,

Flavio

0 Kudos
Reply
5,048 Views
fortunely
Contributor III

Hi Flavio,

Surely there are other options. But I didn't test other programmers.

Maybe you have to valid it by yourself.

This programmer for freescale DSC MCU comes from China, supporting MWCT family.

Ref: http://www.lunkedz.com/?/goods/id-14/index.html  

pastedImage_2.png

0 Kudos
Reply
5,048 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Please consider about CodeWarrior for mcu ver10.x tools.

0 Kudos
Reply
5,048 Views
stproj18
Contributor I

Thank you for your answer but I think I express myself wrong...

I meant hardware programmer, or hardware device for programming in circuit.

0 Kudos
Reply
5,048 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Sorry that I don't understand what you mean about hardware programmer?

Can you give a example?

0 Kudos
Reply
5,048 Views
stproj18
Contributor I

Hi,

I mean a ICSP (in circuit system programmer) to download the firmware in the internal flash without using a bootloader or to write the bootloader.

For example, Microchip has a ICD3 or PICKit3 MPLAB ICD 4 In-Circuit Debugger 

ATMEL has one too Atmel-ICE 

0 Kudos
Reply