Program in LPC932A1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Program in LPC932A1

3,729件の閲覧回数
Mateus92
Contributor I
Does anyone know what software I use to program the LPC932A1?
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

3,501件の閲覧回数
pjp4
Contributor I

Hello

The below are used to program LPC932A1

  lpc900-icp.exe

  lpc900-isp.exe  (bootloader needed)

Would you have the default serial bootloader for 932A1 ?

I need the .BIN file, please?

 

0 件の賞賛
返信

3,713件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Sorry this part is no longer manufacturer thus I can not give you a recommendation for any software 

Regards

 

0 件の賞賛
返信

3,500件の閲覧回数
pjp4
Contributor I

Hello Vincent,

Would you have a default .BIN file with serial bootloader, please?

I need it as I have erased the whole device by mistake. 

I cannot use ISP anymore, just ICP, however, bootloader needs to be restored for ISP.

Best Regards,

Peter

 

0 件の賞賛
返信

3,418件の閲覧回数
pjp4
Contributor I

Hello Everybody,

I got the LPC932A1 programmed from scratch and working w/ factory bootloader with couple of tricks.

I had to compile the bootloader with modified settings and program it with ICP first.

The funny trick is to pull out the ICP prog cable just before SECx are written with 0x06's, which would prevent ISP erase/write later.

Now the LPC932A1 works like the original (ICP and ISP and the desired main code).

Cheers,

Peter

0 件の賞賛
返信