Program in LPC932A1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Program in LPC932A1

3,738 Views
Mateus92
Contributor I
Does anyone know what software I use to program the LPC932A1?
Labels (1)
0 Kudos
Reply
4 Replies

3,510 Views
pjp4
Contributor I

Hello

The below are used to program LPC932A1

  lpc900-icp.exe

  lpc900-isp.exe  (bootloader needed)

Would you have the default serial bootloader for 932A1 ?

I need the .BIN file, please?

 

0 Kudos
Reply

3,722 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Sorry this part is no longer manufacturer thus I can not give you a recommendation for any software 

Regards

 

0 Kudos
Reply

3,509 Views
pjp4
Contributor I

Hello Vincent,

Would you have a default .BIN file with serial bootloader, please?

I need it as I have erased the whole device by mistake. 

I cannot use ISP anymore, just ICP, however, bootloader needs to be restored for ISP.

Best Regards,

Peter

 

0 Kudos
Reply

3,427 Views
pjp4
Contributor I

Hello Everybody,

I got the LPC932A1 programmed from scratch and working w/ factory bootloader with couple of tricks.

I had to compile the bootloader with modified settings and program it with ICP first.

The funny trick is to pull out the ICP prog cable just before SECx are written with 0x06's, which would prevent ISP erase/write later.

Now the LPC932A1 works like the original (ICP and ISP and the desired main code).

Cheers,

Peter

0 Kudos
Reply