Problems with theta calculation in PMSM Vector Control function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems with theta calculation in PMSM Vector Control function

Jump to solution
2,970 Views
peterdufault
Contributor III

I'm still working with something based on AN3206.  I'm trying to figure out what's wrong with my commutation, and I started reading back the theta from the eTPU.  It doesn't make any sense to me.

I have a 4000 count encoder and a motor with two pole pairs.  According to the function description theta = (2 * encoder)/4000, so theta should advance twice for each cycle.  However, it isn't even synchronized with the zero position of the encoder.  See the attached plot.

In etpu_pmsmvc.c scale is set to scale = motor_pole_pairs * 0x1000000 / qd_pc_per_rev; .

Since there was not a "get theta" function I added one like this:

fract24_t fs_etpu_pmsmvc_get_theta(uint8_t channel)

{

    uint32_t *pba;

    pba = fs_etpu_data_ram(channel) + (0x4000 >> 2);

    return (fract24_t)(*(pba + ((FS_ETPU_PMSMVC_THETA_OFFSET) >> 2)));

}

Any ideas?

0 Kudos
Reply
1 Solution
2,722 Views
peterdufault
Contributor III

Never mind.  I had used the PMWmaster channel instead of the PMSMVC_channel and happened to get back that thing that went from -1 to 1.  Now that I've fixed it I get what I expect.

View solution in original post

0 Kudos
Reply
2 Replies
2,722 Views
peterdufault
Contributor III

Well, whatever I'm getting back with that fs_etpu_pmsmvc_get_theta() function it isn't theta.  Even if I stop the motor rotation I get the same -1 to 1 ramp.  I've asked Freescale for the eTPU code that is being generated by the eTPU function selector so I can figure out what's going on.

0 Kudos
Reply
2,723 Views
peterdufault
Contributor III

Never mind.  I had used the PMWmaster channel instead of the PMSMVC_channel and happened to get back that thing that went from -1 to 1.  Now that I've fixed it I get what I expect.

0 Kudos
Reply