PWM Expander PCAL9722HN/Q900MP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PWM Expander PCAL9722HN/Q900MP

2,778 Views
labib_leggett
Contributor I

Hello,

We are using FS32K116LFT0MFMT for a automotive seat massage ECU. We need to drive 24x solenoid or more. Therefore, we need 24x or more PWM channels that can generate 20kHz frequency with a duty cycle of 30% to 100%. 

 

In order to keep same pin-count, we are looking for SPI interfaced PWM expander. It seems PCAL9722HN/Q900MP could be good fits.

Could you please check whether we can generate  20kHz frequency with a duty cycle of 30% to 100% to drive low-side logic level MOSFET? Let me know if you have other options of expanding PWM channel from SPI.

 

Thanks

 

 

0 Kudos
Reply
5 Replies

2,763 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi Labib

From the theory consideration it can support up to 5 MHz of SCLK speed but need software to achieve duty cycle change and 20KHz setting.

0 Kudos
Reply

2,749 Views
labib_leggett
Contributor I

Thank you very much. It has 5MHz SCLK speed. Does it mean I can generate 20kHz PWM channel in all output? How can I calculate maximum allowed PWM frequency on each channel? Is there any app note? I found this in "AMF-IND-T3525.pdf". What is the maximum PWM frequency for PCAL9722HN/Q900MP?

labib_leggett_0-1739193268014.png

 

 

 

0 Kudos
Reply

2,623 Views
guoweisun
NXP TechSupport
NXP TechSupport

According this algorithm,:

Continuous on three Ports
bytes = 25/5MHz=5us=200KHz/2=100KHz

0 Kudos
Reply

2,738 Views
guoweisun
NXP TechSupport
NXP TechSupport

Can you let me know the AMF-IND-T3525.pdf download link?

0 Kudos
Reply

2,708 Views
labib_leggett
Contributor I

I have attached the file herewith. I downloaded the file from NXP website.

0 Kudos
Reply