LPCD problem for NFC Cockpit v8.1.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCD problem for NFC Cockpit v8.1.0

1,278 Views
Shota_py
Contributor I

I am using NFC Cockpit to check LPCD operation.

When a card or metal object is brought near, the following log will be output
INFO:LPCDServicePN5190:Perform LPCD
INFO:LPCDServicePN5190:Load detected
INFO:LPCDServicePN5190:LPCD Calibration
INFO:LPCDServicePN5190:LPCD Calibration successful

 

However, when the iPhone is brought close, an error is output.

WARN:LPCDServicePN5190:Hard resetting the IC. Because LPCD aborted without Card Detection.

Perhaps the problem is the LPCD assistance on the iPhone, but I would like to know how to solve it!

Labels (1)
  • RF

Tags (1)
0 Kudos
Reply
1 Reply

1,262 Views
Fabian_R
NXP TechSupport
NXP TechSupport

Hello, Thank you for your interest in our products.

Please keep in mind that iPhone can only emulate a card with Apple's restrictions. The use of Apple's tools like Apple Pay is out of my support scope. If these tests are performed using Apple Pay, I have to recommend to please contact your DBM or Sales Representative.

Still is possible that the PN5190 could detect the antenna's disturbance when the iPhone is brought close to the antenna and, Wakeup the system. But, there won't be any response from the iPhone to the PN5190 LPCD functionality like an Android HCE or Typical PICC.

Could you please clarify if you are able to calibrate using other devices?

Best Regards,
Fabian
0 Kudos
Reply