PTP default master profile configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PTP default master profile configuration

1,622件の閲覧回数
jibin
Contributor I

jibin_0-1669805198936.pngjibin_0-1669805198936.png

Hi,

The first LS1046A is connected to the grandmaster via the fm1-mac9 optical interface (which serves as a slave to the grandmaster). The first LS1046A fm1-mac3 ethernet interface is used to daisy-chain the second LS1046A.
The first LS1046A fm1-mac3 ethernet interface will serve as a master to the second LS1046A with PTP default profile.
The PTP default profile slave capability has been already enabled in the first LS1046A. Now we need to create a second instance of ptp4l as a master in first LS1046A with PTP default profile.
Could someone kindly assist us or provide us the PTP default master profile configuration?

Regards,

Jibin

タグ(2)
0 件の賞賛
返信
1 返信

1,602件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

The first LS1046A board works as a boundary clock, you can refer to LSDK document "Chapter 8.7.5.2: Boundary clock verification" for the details how to run a boundary clock.

0 件の賞賛
返信