Hi,
The first LS1046A is connected to the grandmaster via the fm1-mac9 optical interface (which serves as a slave to the grandmaster). The first LS1046A fm1-mac3 ethernet interface is used to daisy-chain the second LS1046A.
The first LS1046A fm1-mac3 ethernet interface will serve as a master to the second LS1046A with PTP default profile.
The PTP default profile slave capability has been already enabled in the first LS1046A. Now we need to create a second instance of ptp4l as a master in first LS1046A with PTP default profile.
Could someone kindly assist us or provide us the PTP default master profile configuration?
Regards,
Jibin
The first LS1046A board works as a boundary clock, you can refer to LSDK document "Chapter 8.7.5.2: Boundary clock verification" for the details how to run a boundary clock.