PTN36043 DE/OS/EQ setting

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PTN36043 DE/OS/EQ setting

跳至解决方案
2,953 次查看
jackylu
Contributor II

Dear Sir,

Good day,

For my application,

PTN36043 very close  with Processor Qualcomm SDX20.

Any comment for DE/OS/EQ setting in Processor side?

Thanks.

0 项奖励
回复
1 解答
2,789 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

By default, using the open (default) settings should work. (CHx_SETx = OPEN)

But for the first build, I would suggest to still have the pull up and pull down resistor footprints in place on the setting pins, just in case the OPEN settings are not optimum.

 

If this your new design you can consider about PTN36043A part, it will be more USB-C  compliant.

The difference between the PTN36043 and PTN36043A is that

  • In PTN36043, the unused (or un-selected) channels SSTX and SSRX are tie to low ohmic
  • In PTN36043A, the unused (or un-selected) channels SSTX and SSRX are tie to high ohmic

 

The reason is to be comply with Type-Cs safe state requirement. 

 

 

在原帖中查看解决方案

1 回复
2,790 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

By default, using the open (default) settings should work. (CHx_SETx = OPEN)

But for the first build, I would suggest to still have the pull up and pull down resistor footprints in place on the setting pins, just in case the OPEN settings are not optimum.

 

If this your new design you can consider about PTN36043A part, it will be more USB-C  compliant.

The difference between the PTN36043 and PTN36043A is that

  • In PTN36043, the unused (or un-selected) channels SSTX and SSRX are tie to low ohmic
  • In PTN36043A, the unused (or un-selected) channels SSTX and SSRX are tie to high ohmic

 

The reason is to be comply with Type-Cs safe state requirement.