XQ1TXH5 charge problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

XQ1TXH5 charge problem

1,000件の閲覧回数
milimhuang
Contributor I

Hi Sir,
We use your company's NXQ1TXH5 produced in week45 of 2002 and stop charging when the current slowly rises above 1A.

Your company's answer is as follows:

---------------------------------------------------------------------------------------------------------------

Customer could start with those steps to narrow down what is causing the fault: 

(Try each one individually, (after each go back to configuration before changes.)

 

  1.      Replace resistor connected to CNF1 pin with short, 0 Ohm.

This will turn off SPR static power reduction and SPL smart power limiting. 

 

  1.      Replace resistor connected to CNF3 pin with short, 0 Ohm.

This will turn off FOD foreign object detection.Wireless Connectivity

 

  1.      Short NTC pin to ground.

This will turn off external NTC sensing and 85 deg C power reduction threshold.

 ---------------------------------------------------------------------------------------------------------------- 
However, these tests are not improved.
I short NTC3 pin to ground and it can charge.
What is the correct solution?

0 件の賞賛
返信
0 返答(返信)