PSI5 set sensor 2 address using daisy chain mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PSI5 set sensor 2 address using daisy chain mode

Jump to solution
2,395 Views
xushaotian
Contributor I

Why is the command to set the address of sensor2  0x2AAE instead of 0x28AF (command is 0x28AF on PSI5 manual)? 

on your AN12776_PSI5NormalMode manual ,used 0x2AAE on Page 24.

 

0 Kudos
Reply
1 Solution
2,381 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello xushaotian,

I hope all is great with you. Thank you for using the NXP communities.

The PSI5 Programing Mode Entry Settings is shown below.

diazmarin09_0-1688582194895.png

 

Based on the AN12776 document, the address of the Sensor2=010.

(Start bits = 0h2) + (Sensor Address =0hA)

I hope this information helps.

Regards,

David

View solution in original post

0 Kudos
Reply
2 Replies
2,382 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello xushaotian,

I hope all is great with you. Thank you for using the NXP communities.

The PSI5 Programing Mode Entry Settings is shown below.

diazmarin09_0-1688582194895.png

 

Based on the AN12776 document, the address of the Sensor2=010.

(Start bits = 0h2) + (Sensor Address =0hA)

I hope this information helps.

Regards,

David

0 Kudos
Reply
2,364 Views
xushaotian
Contributor I

Ok ,i see.

Thank you!

0 Kudos
Reply