PSI5 set sensor 2 address using daisy chain mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PSI5 set sensor 2 address using daisy chain mode

ソリューションへジャンプ
2,390件の閲覧回数
xushaotian
Contributor I

Why is the command to set the address of sensor2  0x2AAE instead of 0x28AF (command is 0x28AF on PSI5 manual)? 

on your AN12776_PSI5NormalMode manual ,used 0x2AAE on Page 24.

 

0 件の賞賛
返信
1 解決策
2,376件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello xushaotian,

I hope all is great with you. Thank you for using the NXP communities.

The PSI5 Programing Mode Entry Settings is shown below.

diazmarin09_0-1688582194895.png

 

Based on the AN12776 document, the address of the Sensor2=010.

(Start bits = 0h2) + (Sensor Address =0hA)

I hope this information helps.

Regards,

David

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,377件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello xushaotian,

I hope all is great with you. Thank you for using the NXP communities.

The PSI5 Programing Mode Entry Settings is shown below.

diazmarin09_0-1688582194895.png

 

Based on the AN12776 document, the address of the Sensor2=010.

(Start bits = 0h2) + (Sensor Address =0hA)

I hope this information helps.

Regards,

David

0 件の賞賛
返信
2,359件の閲覧回数
xushaotian
Contributor I

Ok ,i see.

Thank you!

0 件の賞賛
返信