PSI5 set sensor 2 address using daisy chain mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PSI5 set sensor 2 address using daisy chain mode

跳至解决方案
2,398 次查看
xushaotian
Contributor I

Why is the command to set the address of sensor2  0x2AAE instead of 0x28AF (command is 0x28AF on PSI5 manual)? 

on your AN12776_PSI5NormalMode manual ,used 0x2AAE on Page 24.

 

0 项奖励
回复
1 解答
2,384 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello xushaotian,

I hope all is great with you. Thank you for using the NXP communities.

The PSI5 Programing Mode Entry Settings is shown below.

diazmarin09_0-1688582194895.png

 

Based on the AN12776 document, the address of the Sensor2=010.

(Start bits = 0h2) + (Sensor Address =0hA)

I hope this information helps.

Regards,

David

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,385 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello xushaotian,

I hope all is great with you. Thank you for using the NXP communities.

The PSI5 Programing Mode Entry Settings is shown below.

diazmarin09_0-1688582194895.png

 

Based on the AN12776 document, the address of the Sensor2=010.

(Start bits = 0h2) + (Sensor Address =0hA)

I hope this information helps.

Regards,

David

0 项奖励
回复
2,367 次查看
xushaotian
Contributor I

Ok ,i see.

Thank you!

0 项奖励
回复