PNEV7642A cannot write NxpNfcCockpit Firmware

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PNEV7642A cannot write NxpNfcCockpit Firmware

2,677 次查看
MikeAtPhantom
Contributor I

After putting PNEV7642A into mass storage mode, erase CRP_00.BIN, but when I write NxpNfcCockpit Firmware the device reverts to CRP_00.BIN.

标签 (1)
标记 (2)
0 项奖励
回复
4 回复数

1,386 次查看
pberveiller
Contributor II

Hello,

I have a similar issue. I’m using a PN7642 C101 on my custom board.

When I power up the board, a Mass Storage device appears.
I delete the file CRP_00.BIN and replace it with my own .bin file.

However, after powering up the board again, the PN7642 still shows up in Mass Storage mode.
I also tried with another computer, but the result is the same.

Do you have any advice or suggestions?

0 项奖励
回复

2,663 次查看
danielchen
NXP TechSupport
NXP TechSupport

 

I encountered this issue before. It is because my IT department imposed some restrictions on the USB port for some security reasons.  I can not write/delete any files from USB ports.  I would suggest you check whether you have full control over the USB port on your PC.

 

Regards

Daniel

0 项奖励
回复

2,658 次查看
MikeAtPhantom
Contributor I

Hi Daniel,

I do not have an IT department. I turned off the firewall, checked the registry and BIOS, the USB ports are unrestricted and fine for other options. Do I need to turn off boot from USB option off?

Thanks.

Mike

0 项奖励
回复

2,652 次查看
danielchen
NXP TechSupport
NXP TechSupport

Is it possible to try with another PC?

0 项奖励
回复