Fully Connected layer conversion showing internal error in neutron converter in iMX95 Verdin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fully Connected layer conversion showing internal error in neutron converter in iMX95 Verdin

1,411 Views
PoojaSk
Contributor II

Hi,

Tried converting classifier models such as InceptionV3, Resnet50 and Mobilenetv3Small using neutron converter targeting iMX95. On converting fully connected layer to ConvertFullyConnectedToConv, it is showing internal error. 

PoojaSk_2-1747980635221.png

 

PoojaSk_0-1747979255547.png

 

This is the fully connected layer which is not getting converted. But this layer does not violate any of the constraints mentioned in the section 5.9.7 FULLY_CONNECTED constraints of UG.

PoojaSk_1-1747979421074.png

 

 How can we fix this issue as I am unable to run any classifier with fully connected layer in iMX95 Neutron NPU.

0 Kudos
Reply
2 Replies

1,220 Views
varshilg
Contributor II

Hi Pooja,

I am also facing this issue that fully_connected layer not able to convert into neutron graph.

Did you find any solution of it?

Regards,

Varshil

0 Kudos
Reply

1,394 Views
joanxie
NXP TechSupport
NXP TechSupport

i.mx95 is still under pre-prodcution, we couldn't share detailed technical information on the public community, pls contact local DFAE to get further support

0 Kudos
Reply