PNEV7642A cannot write NxpNfcCockpit Firmware

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PNEV7642A cannot write NxpNfcCockpit Firmware

2,633件の閲覧回数
MikeAtPhantom
Contributor I

After putting PNEV7642A into mass storage mode, erase CRP_00.BIN, but when I write NxpNfcCockpit Firmware the device reverts to CRP_00.BIN.

ラベル(1)
タグ(2)
0 件の賞賛
返信
4 返答(返信)

1,342件の閲覧回数
pberveiller
Contributor II

Hello,

I have a similar issue. I’m using a PN7642 C101 on my custom board.

When I power up the board, a Mass Storage device appears.
I delete the file CRP_00.BIN and replace it with my own .bin file.

However, after powering up the board again, the PN7642 still shows up in Mass Storage mode.
I also tried with another computer, but the result is the same.

Do you have any advice or suggestions?

0 件の賞賛
返信

2,619件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

 

I encountered this issue before. It is because my IT department imposed some restrictions on the USB port for some security reasons.  I can not write/delete any files from USB ports.  I would suggest you check whether you have full control over the USB port on your PC.

 

Regards

Daniel

0 件の賞賛
返信

2,614件の閲覧回数
MikeAtPhantom
Contributor I

Hi Daniel,

I do not have an IT department. I turned off the firewall, checked the registry and BIOS, the USB ports are unrestricted and fine for other options. Do I need to turn off boot from USB option off?

Thanks.

Mike

0 件の賞賛
返信

2,608件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Is it possible to try with another PC?

0 件の賞賛
返信