PNEV7642A cannot write NxpNfcCockpit Firmware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PNEV7642A cannot write NxpNfcCockpit Firmware

2,685 Views
MikeAtPhantom
Contributor I

After putting PNEV7642A into mass storage mode, erase CRP_00.BIN, but when I write NxpNfcCockpit Firmware the device reverts to CRP_00.BIN.

Labels (1)
Tags (2)
0 Kudos
Reply
4 Replies

1,394 Views
pberveiller
Contributor II

Hello,

I have a similar issue. I’m using a PN7642 C101 on my custom board.

When I power up the board, a Mass Storage device appears.
I delete the file CRP_00.BIN and replace it with my own .bin file.

However, after powering up the board again, the PN7642 still shows up in Mass Storage mode.
I also tried with another computer, but the result is the same.

Do you have any advice or suggestions?

0 Kudos
Reply

2,671 Views
danielchen
NXP TechSupport
NXP TechSupport

 

I encountered this issue before. It is because my IT department imposed some restrictions on the USB port for some security reasons.  I can not write/delete any files from USB ports.  I would suggest you check whether you have full control over the USB port on your PC.

 

Regards

Daniel

0 Kudos
Reply

2,666 Views
MikeAtPhantom
Contributor I

Hi Daniel,

I do not have an IT department. I turned off the firewall, checked the registry and BIOS, the USB ports are unrestricted and fine for other options. Do I need to turn off boot from USB option off?

Thanks.

Mike

0 Kudos
Reply

2,660 Views
danielchen
NXP TechSupport
NXP TechSupport

Is it possible to try with another PC?

0 Kudos
Reply