PICO-IMX8 USB 2.0 controller issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PICO-IMX8 USB 2.0 controller issue

1,798 Views
jahnaviguvvala
Contributor I

Hi,

 

I am facing an issue with USB 2.0 controller in the PICO-IMX8 SOM.

I am using this USB for audio device with EN1 IN and EN1 OUT for mic and speakers. I connect this audio device to the host pc , through a USB hub. Here, whenever I connect a new device to the USB hub, my audio device stops receiving OUT packets. IN transactions are happening fine. I debugged it and understood that USB_ENDPTCOMLETE register shows whether an endpoint completed the request or not. It seems that this bit is not getting asserted. Which means , OUT transaction is not getting completed even if transfer-descriptors are present.

Can someone help me with what are the cases when endpoint stops receiving packets? 

P.S: We observed in USB sniffer, host is sending the packets. Its the device that is not receiving them.

 

Appreciate your help,

 

Thanks,

Jahnavi.

0 Kudos
Reply
2 Replies

1,787 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jahnavi

 

in general, supported usb functionality is described in sect.4.9 USB i.MX Linux Reference Manual​

so I am not sure if usb audio could be well supported:

•Host mode-Supports HID (Human Interface Devices), MSC (Mass Storage Class)
• Peripheral mode-Supports MSC, and CDC (Communication Devices Class) drivers,

which include Ethernet and serial support.

 

Best regards
igor

0 Kudos
Reply

1,777 Views
jahnaviguvvala
Contributor I

Hi Igor,

 

From the iMX8MINI reference maual, https://www.nxp.com/webapp/Download?colCode=IMX8MMRM

It is mentioned that the 2.0 OTG controller can be used for isochronous transfers also.

We are trying to use this controller driver with USB audio gadget driver to achieve audio functionality.

Please let me know if i am missing something..

 

Thanks,

Jahnavi.

 

0 Kudos
Reply