PF3000 input power

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PF3000 input power

946 次查看
noamweidenfeld
Contributor I

Hi,

I am using the SMARC standard for SOM applications. The input power requirements are 3.0V to 5.25V.

Can I use the PF3000 for such input requirements? (I failed to understand the sentence " Input voltage range: 2.8 V to 4.5 V or 3.7 V to 5.5 V")

Thanks

Noam

0 项奖励
回复
0 回复数