PCF2129 SDO and CLKOUT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCF2129 SDO and CLKOUT

1,710 次查看
mlibhart
Contributor I

Really simple question from a hobbyist.  Is it ok to let SDO (serial data out) and the clkout float on the PCF2129 RTC if I'm not using either, or should they be tied one way or the other?  I'll be using I2C so don't need the SDO.

Thanks.

0 项奖励
回复
3 回复数

1,590 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Matthew,

The SDO and CLKOUT pins of the PCF2129 device are output functions.  It is okay to leave output pins floating.

Best regards,

Tomas

0 项奖励
回复

1,590 次查看
fatihozen
Contributor IV

Hi, I have similar question, I won't use TS, SDO, INT and CLKOUT pins and ESD protection is very important on my side. What do you suggest for these pins connections ? I think it is better choice to connect them somewhere via resistors than letting float, but I need an advice here.

0 项奖励
回复

1,590 次查看
mlibhart
Contributor I

Hi Tomas,

Thanks so much for the quick reply.  Really appreciate it.

0 项奖励
回复