PCF2129 SDO and CLKOUT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCF2129 SDO and CLKOUT

741 Views
mlibhart
Contributor I

Really simple question from a hobbyist.  Is it ok to let SDO (serial data out) and the clkout float on the PCF2129 RTC if I'm not using either, or should they be tied one way or the other?  I'll be using I2C so don't need the SDO.

Thanks.

0 Kudos
Reply
3 Replies

621 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Matthew,

The SDO and CLKOUT pins of the PCF2129 device are output functions.  It is okay to leave output pins floating.

Best regards,

Tomas

0 Kudos
Reply

621 Views
fatihozen
Contributor IV

Hi, I have similar question, I won't use TS, SDO, INT and CLKOUT pins and ESD protection is very important on my side. What do you suggest for these pins connections ? I think it is better choice to connect them somewhere via resistors than letting float, but I need an advice here.

0 Kudos
Reply

621 Views
mlibhart
Contributor I

Hi Tomas,

Thanks so much for the quick reply.  Really appreciate it.

0 Kudos
Reply