what are control pins in mfrc522

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what are control pins in mfrc522

689 Views
mnfsoft
Contributor I

you refer to your datasheet by the name "control pins" in section 8.1.1; I.e. this is a lazy written document with poor or no  revision I mean I do not see many chips like this plus what is the harm of mentioning their name; hence this datasheet is getting hard to understand each time I begin to read it and try to understand it!

Tags (2)
0 Kudos
Reply
1 Reply

644 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

 See below, please!

pastedImage_1.png

Using UART interface:  I2C PIN =0 && EA PIN=0

Using SPI interface : I2C PIN =0 && EA PIN=1

Using I2C-BUS interface: I2C PIN =1 && EA PIN=X

Have a nice day!

BR,

NXP TIC Weidong Sun

0 Kudos
Reply