PCAL6524 QFN Exposed Pad Connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCAL6524 QFN Exposed Pad Connection

Jump to solution
1,150 Views
mmWaver
Contributor I

Can someone please confirm if PCAL6524 QFN32 package's center exposed pad can/should be connected to ground?

Thanks!

Tags (2)
0 Kudos
Reply
1 Solution
1,136 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Paul,

The exposed pad underneath the PCAL6524HE (HUQFN32) is not internally connected to any pin. It can be left floating, but for better thermal performance it is recommended to connect it to the GND.

The exposed pad outline and the recommended footprint can be found at:

https://www.nxp.com/docs/en/package-information/SOT1426-1.pdf

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
2 Replies
1,121 Views
mmWaver
Contributor I

Thank you Tomas for your reply!

0 Kudos
Reply
1,137 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Paul,

The exposed pad underneath the PCAL6524HE (HUQFN32) is not internally connected to any pin. It can be left floating, but for better thermal performance it is recommended to connect it to the GND.

The exposed pad outline and the recommended footprint can be found at:

https://www.nxp.com/docs/en/package-information/SOT1426-1.pdf

Best regards,

Tomas

0 Kudos
Reply