PCAL6524 Libbary file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCAL6524 Libbary file

1,948 Views
MRD3326
Contributor I

Hello,

I am working on PCAL6524.I am interfacing it with STM32h7.I need the library file of that, can you please provide me library.

Tags (1)
0 Kudos
Reply
4 Replies

1,927 Views
guoweisun
NXP TechSupport
NXP TechSupport

what kind of library do you need?

 

 

0 Kudos
Reply

1,886 Views
MRD3326
Contributor I

I have to interface with stm32.For arduino board the library is available that kind of liberty I need for stm32.

0 Kudos
Reply

1,925 Views
MRD3326
Contributor I

I have configure with it stm32.I need to read the voltage of 15v which are connected to one port pin. So how can access that register. They provide Linux driver or ardiuio libarary. That kind of libabry I need so I can read the register. 

0 Kudos
Reply

1,926 Views
MRD3326
Contributor I

I have configure with it stm32.I need to read the voltage of 15v which are connected to one port pin. So how can access that register. They provide Linux driver or ardiuio libarary. That kind of libabry I need so I can read the register. 

0 Kudos
Reply