PCAL6524 Libbary file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCAL6524 Libbary file

1,895 次查看
MRD3326
Contributor I

Hello,

I am working on PCAL6524.I am interfacing it with STM32h7.I need the library file of that, can you please provide me library.

标记 (1)
0 项奖励
回复
4 回复数

1,874 次查看
guoweisun
NXP TechSupport
NXP TechSupport

what kind of library do you need?

 

 

0 项奖励
回复

1,833 次查看
MRD3326
Contributor I

I have to interface with stm32.For arduino board the library is available that kind of liberty I need for stm32.

0 项奖励
回复

1,872 次查看
MRD3326
Contributor I

I have configure with it stm32.I need to read the voltage of 15v which are connected to one port pin. So how can access that register. They provide Linux driver or ardiuio libarary. That kind of libabry I need so I can read the register. 

0 项奖励
回复

1,873 次查看
MRD3326
Contributor I

I have configure with it stm32.I need to read the voltage of 15v which are connected to one port pin. So how can access that register. They provide Linux driver or ardiuio libarary. That kind of libabry I need so I can read the register. 

0 项奖励
回复